Cancel
Showing results for 
Search instead for 
Did you mean: 

Save Manufacturing Preferences

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi!

 

Why in some computers the Configuration File\cam_general.dat and Template set\cam_general.opt take default option Although I have a user customization?

 

And i other computers take automatically my personal configuration?

 

Thanks

Best regards

Ivan

3 REPLIES 3

Re: Save Manufacturing Preferences

Legend
Legend

Help -> Nx log file

 

Now , look for the variable UGII_CAM_CONFIG_DIR and UGII_CAM_TEMPLATE_SET_DIR

Normally 2 variables should show the path of your customization

If it is not the case , I advise you to look this way NXcustom Utilities , a lot of information to customize your CAM environment

Production: NX11.0.2.7,VERICUT 8.1.2
Development: Tcl/Tk, Gnuplot
www.adgroupe.com

Re: Save Manufacturing Preferences

Valued Contributor
Valued Contributor

You are not logged in as user on computer

 

Your files containing your preferences are not located in the computer your using with NX installed.

 

 

C:\Users\tedwards\AppData\Local\Siemens\NX100

is where system setting files will be located on the Computer folder.

 

Your .dlx, .krx, .pax, .txt, .dpv, .xsl, and .mtx file extentions are located in this folder.

 

As for the Configuration, Postprocessor, Template_Part, Template_Set folders and files must be located  and mapped to there correct locations.

EDS UG V3 -UG V15 UNIX; UGS UG V6 -UG V19 - NX-NX5 UNIX/MS;
Siemens NX6-NX10; NX11; NX12; NX1847 MS

Re: Save Manufacturing Preferences

Genius
Genius

mkn is right.

You may watch at the customer defaults for Manufacturing. Quite at the beginning there's the Use Configuration based on Role setting. When is is set to on NX CAM uses the configuration that has been saved in the role.

Best wishes,
Joachim

In production NX 12.0.1.7 MP4
In testing NX 12.0.2.9 MP5

Learn online





Solution Information