Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Save Tool Axis at Any Given Point in Replay

Pioneer
Pioneer

Is it possible in NX10 or 11 to save the point vector of the Tool Axis at any given point in the replay(Verify)?

 

It's nice sometime to check the tool back to a surface.

 

Cyl

3 REPLIES 3

Re: Save Tool Axis at Any Given Point in Replay

Phenom
Phenom
Other option , you can take the measure distance , and check tool body to surface
Production: NX11.0.2.7,VERICUT 8.1.2
Development: Tcl/Tk, Gnuplot
www.adgroupe.com

Re: Save Tool Axis at Any Given Point in Replay

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

In NX 11 with the tool path visualization dialog open you can select analysis- measure distance and activate Create Output Geometry - this will can create a line between two points.  

 

This was in previous versions of NX but somehow got dropped from NX10.  I am glad to see it is back.

 

You can also orient the WCS to the tool.  Just make sure the selection scope is set to entire assembly.

 

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Save Tool Axis at Any Given Point in Replay

Pioneer
Pioneer

Thank you John and MKN.

 

I don't see 'Create Ouput Geom.' in NX11.01, but I do see 'Between Componet Sets' under Measure Distance and this works just as well!

 

Cyl

Learn online





Solution Information