Cancel
Showing results for 
Search instead for 
Did you mean: 

Selecting the tool position during machining

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello ,
I encountered a turret problem when working from two directions on one revolver. The drawing is a revolver that has 12 positions and can be machined both toward the main spindle and the sub-spindle, and the M764 and M765 function is selected on which side the tool is machining. Would not anyone have suggested how to define that the M765 function should be machined to the sub spindle? Tool number 1 can handle both the main spindle and sub-spindle.

 

MILL_TURN.png

 

 

Learn online





Solution Information