Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Sequential drilling with bore cycles

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi,
We can only use interrupted option when motion output selected as single moves. The bore cycle is in the machine cycle.
Is there a way to add a boring cycle to the sequential drilling operation.

 

 

1 REPLY

Re: Sequential drilling with bore cycles

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'd have to see the documentation of the machine's boring cycle that you want to use.

All the ones I am familiar with (Okuma, Fanuc, Mazak, Siemens 840D) only go (once) to the bottom of the hole, then retract completely out - they don't "go slow thru material" *and* "go fast thru air".

 

If that's what you want (a G8x or G7x cycle), don't use the Sequential drill operation - use a "regular" bore cycle.

Legacy PTP operations ignore all the gaps.

I'm not sure what to do that in holemaking (assuming it is possible) to ignore the gaps (I haven't played with it that much...)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information