Cancel
Showing results for 
Search instead for 
Did you mean: 

Setting the tool holder for two tools

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello everyone,

Could anyone advise me how to properly set up in kinematic machine use on a turret lathe holder for two tools? It is a lathe with an anti-spindle. The tools that are on the main spindle side have numbers 1-16 and the tools on the counter spindle have 17-46. Always, if I choose tool T33 and I want to work on the counter, I'm working on the T3 tool.

 

 

 

 

2 REPLIES 2

Re: Setting the tool holder for two tools

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Multi tool support is planned, but not implemented yet.

I think there is a heavy load of voodoo needed to accomplish this in the current NX releases.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Setting the tool holder for two tools

Siemens Phenom Siemens Phenom
Siemens Phenom

You can have a look into this example:

sim15_millturn_setup_sinumerik_mm_dual_sync.prt

 

Here the NC code always position the turret with the main pocket number, which include a device object with two pockets for the cutter left/right. The activation of the one or the other cutter (including the length compensation) is done via D1 or D2 the given adjust register in the cutter object.

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information