Cancel
Showing results for 
Search instead for 
Did you mean: 

Shop Doc: Cannot Get Coolant Mode and Part Revision

Valued Contributor
Valued Contributor

Hello there,

 

I am editing the shop doc excel template so that I can get the coolant mode and the part revision.

 

For coolant mode, I set it in UDE start event. I tried setting the UDE event in the operation or the tool. I tried using the following variable to get it, but failed.

 

mom_coolant_mode

I couldn't find this variable in the Review Tool as well. 

 

As for part revision, I tried the following two variables, but couldn't get the value. I could find these two variables in the Review Tool.

 

mom_attr_PART_DB_PART_REV

mom_db_part_rev

 

Thanks,

Kai

2 REPLIES 2

Re: Shop Doc: Cannot Get Coolant Mode and Part Revision

UDE mom variables are only available in postprocessing, not shopdocs. One reason why many users generate their shopdocs from their posts.

 

Is the part revision a part attribute? Select the part in the ANT, MB3 > Properties and be sure. 

Part attributes are set as mov variables mom_attr_PART_*

Mark Rief
Retired Siemens

Re: Shop Doc: Cannot Get Coolant Mode and Part Revision

Valued Contributor
Valued Contributor

Thanks, Mark. We used to create customized tool sheet through post. The reason why we are working on the Shop Doc now is that Shop Doc provides pictures of the setup and each operation. 

 

Is there a way to insert those pictures through posts by coding? Or is there a way to generate pictures through posts?

 

Thanks,

Kai

Learn online





Solution Information