Cancel
Showing results for 
Search instead for 
Did you mean: 

Shop-Doc output with PP-run

Hi,

 

i´m using NX10 and editing some existing PPs with PostBuilder. 

Now my question is:

Is there any possibility to output the ShopDoc out of the PP? So, that i just have to click on the PP-Button, select my PP, browse to output destination, and by clicking "OK" there will be the ShopDoc and the NC-Code in the destination folder.

That would be great Smiley Happy

 

Best wishes from Germany Smiley Wink 

1 REPLY 1

Re: Shop-Doc output with PP-run

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

MOM_do_template_file abc.tpl

 

will run the shop docs .tpl

 

Not sure how to trigger the right tl file (you may need to "source" it into the posts tcl file

 

Note you may want to create a special "post" to just run the shop docs, then use MOM_run_postprocess in your main post's tcl file to run the "do the shop doc" post (this way, all the mom variables should remain correct for the actual posting)

 

Another option is to use a journal to do posting, and the journal can (separate commands, but one journal) post the code & generate the shop docs.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information