Cancel
Showing results for 
Search instead for 
Did you mean: 

Show Pictures in Dialog Boxes

Pioneer
Pioneer

Show Pictures in Dialog Boxes

 

Hay maybe irrelevant thing… but anyway…

Why there is no »Pictures in Dialog Boxes« in CAM when in e.g. »Cutting parameters«

There is checkbox in Customers defaults: »Show Pictures in Dialog Boxes”, (It says: This option determines whether or not pictures are displayed in the Cutting Parameters and Non Cutting Moves dialog boxes.) but pictures are not “permanently” showing, just a preview when mouse is over specific parameter.

In e.g NX 8.5 there are pictures – permanently displaying,

 

Is there any way the pic. would be “permanent” as in NX 8.5

Thnx.

 

Best

Opl.

2 REPLIES 2
Highlighted

Re: Show Pictures in Dialog Boxes

Genius
Genius

Hello,

 

It was an enhancement that came in at NX9 so you only see the pictures when selecting or hoovering over the setting you are looking at allowing a smaller box taking up less of the screen, I don't think there is a way to set them as was in eariler releases but I may be wrong.

Regards

Dave
NX10.0.3MP13
NX11.0.1
Production
TC10
Vericut 7.3,7.4.1,8.0.2

Re: Show Pictures in Dialog Boxes

@CAM_Jockey is correct.

 We changed these to "tool tips" in NX 8.5.

You can see the details under "Cutting Parameters and Non Cutting Moves dialog box enhancements" in the NX 8.5 What's New Guide

Mark Rief
Retired Siemens

Learn online





Solution Information