Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Sim 15 for Fanuc. NX 8.5. Trouble with simulation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello all.

I have trouble with simulation in Sim 15 Fanuc machine in NX 8.5

When I have to add mill operation in lower turret my machin after this operation doesn't change tool in simulation.
I do this in NX 9 and NX 10 and there changed tool work.

Maybe somebody know, how to solve this problem?

2 REPLIES 2

Re: Sim 15 for Fanuc. NX 8.5. Trouble with simulation

Siemens Phenom Siemens Phenom
Siemens Phenom

No idea yet, is the NC code the same as in NX9 and NX10?

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Sim 15 for Fanuc. NX 8.5. Trouble with simulation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Yes, the NC code is the same

Learn online





Solution Information