Cancel
Showing results for 
Search instead for 
Did you mean: 

Sim15 Turret Setup for the Kinematic Model

Genius
Genius

I am interested in understanding why the Sim15 turret is set up the way it is, with 2 axes seemingly doing the same thing.  When I go into the TURRET Axis, it rotates the turret.  When I go into the LOWER_SPINDLE or C2 Axis it does the same thing.  The difference being that LOWER_SPINDLE is set up as a _DEVICE and the Axis Type is Spindle.  Would it all still work if we removed the TURRET machine component?

Capture.PNG

 

Thank you,

Jesse

3 REPLIES 3

Re: Sim15 Turret Setup for the Kinematic Model

Siemens Phenom Siemens Phenom
Siemens Phenom
Hi Jesse,

good question. I´dont know why and I don´t see any need to have the axis movement and different definition in both components. TURRET axis is nowhere used as axis, as far as I see. Maybe it´s in due to historical reasons.

ThomasF

Re: Sim15 Turret Setup for the Kinematic Model

Genius
Genius

Thanks for the reply Thomas!  I'll try without the redundancy and report back if it doesn't work.

Re: Sim15 Turret Setup for the Kinematic Model

Siemens Phenom Siemens Phenom
Siemens Phenom

I do see one place where TURRET is used to position the turret to the correct pocket position during tool change.

Why we did it that way I can not remember ....

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information