Cancel
Showing results for 
Search instead for 
Did you mean: 

Simple Post Processor question

Creator
Creator

How do you get to create a postprocessor? Is the program within NX, or is it a seperate program? I found Post Configurator in the command search, but for some reason the command is not available. Is the post builder an additional add on to NX? Thanks for any input.

3 REPLIES

Re: Simple Post Processor question

Esteemed Contributor
Esteemed Contributor

Post configurator is shipping with NX and is installed if the typical installation is used.

You need a CAM license and a nx_post_config_adv license, which is part of all newer CAM bundles.

What license bundle do you have?

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community

Re: Simple Post Processor question

Esteemed Contributor
Esteemed Contributor

The older method is to use Post Builder.

This is started separately from NX (alster as needed for your NX version):

"Windows" menu -> All programs -> Siemens NX 10.0 -> Manufacturing -> Post builder

 

Post Configurator is the "go forward" posting technology, but I haven't had a chance to play with it yet, so I don't know how it compares to Post Builder.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Simple Post Processor question

Creator
Creator
This is the answer I was looking for. Thanks a lot! Good to know about where the technology is heading though.

Learn online





Solution Information