Cancel
Showing results for 
Search instead for 
Did you mean: 

Simulating Fanuc subprogram.

Pioneer
Pioneer
Is anyone having any luck simulating an external gcode file that contains subprograms in Machine Simulator? The programs I am trying to simulate have a M98P#### and then have a O#### at the bottom of the file with a M99 to return it back to the main program. This is all done in the same gcode file.
I keep getting an error that says the program can't be found once it calls the M98 line.
NX 12.0.0 PB 12.0.0
9 REPLIES

Re: Simulating Fanuc subprogram.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello

 

for simulation with subprograms and cycles it is needed to have each program in a separate file.

One file for the main program with the M98 call and a subprogram file ####.ptp. In the subprogram file the first lien is then O####.

Then it will work.

 

It will not work if all program are in one file.

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Simulating Fanuc subprogram.

Valued Contributor
Valued Contributor

Please put in an enchancement request. I don't have much experience using the simulation, but I would think that if the real machine can do something than the one on the computer should be able do it too?

Using NX 8.0.3.4

Re: Simulating Fanuc subprogram.

Pioneer
Pioneer

I agree and I will put one in. I was able to get it to work using Tom's method. The main issue that I have is now we are not simulating the actual g-code that is run on the floor. Yes I am only copying and pasting out the subs but there is still some room for error.

NX 12.0.0 PB 12.0.0

Re: Simulating Fanuc subprogram.

Pioneer
Pioneer

Hi is there any enhancement done on M98 P working as I am also facing the same issue in simulation it says cant find the subprogram.

Re: Simulating Fanuc subprogram.

Gears Phenom Gears Phenom
Gears Phenom

On a Fanuc control, when the NC file is loaded it puts the Sub programs into separate files in the control. 

 

John Joyce, Manufacturing Engineer,
Senior Aerospace Connecticut
www.senioraeroct.com
Production: NX11.0.2.7, Vericut 8.0.3
Development: Tcl/Tk
Testing NX12.0

Re: Simulating Fanuc subprogram.

Pioneer
Pioneer

Hi ,,

 

So I have define a subprogram file named 71.prg(kept this file in subprogram folder of cse_drivers) in case of M98 P71 but the Simulation gives error :"saying program O071 not found ".

 

 

I tried with P1 also not working at all.

 

Regards

Keerti

Re: Simulating Fanuc subprogram.

Siemens Phenom Siemens Phenom
Siemens Phenom

Please name the file:

O0071.prg

 

Hope that helps

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Simulating Fanuc subprogram.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And in case it isn't obvious...(it took me a second to realize...)

 

"letter Oh"-"number zero"-"number zero"-"seven"-"one"

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Simulating Fanuc subprogram.

Pioneer
Pioneer
working thankyou

Learn online





Solution Information