Cancel
Showing results for 
Search instead for 
Did you mean: 

Sinumerik parser comment "()" and not ";"

Experimenter
Experimenter

For a "Sinumerik 880 T" I would have the commentary sentence instead of ";" parse with "()".
Is there a way to do this in the MCF?

 

Thanks for possible solutions

1 REPLY

Re: Sinumerik parser comment "()" and not ";"

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

I see two options.

 

1.) Use the CSE command "CSEPreprocessLine" but be careful. It is suggested for cases without any other possibility. Keep in mind that it has a performance impact.

Search for this command in the forum. There are some threads about it and how to use it.

 

2.) Use Fanuc CCF if the nc code consists of G-M codes only. May this could lead to other problems but could be a workaround


Thomas

Learn online





Solution Information