Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Tools - Length available in posting?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

NX 10.0.3.5 MP19

Tring to figure out if a solid tool's length (total length from back of holder to tip of ball)  is available in posting.

 

E.g. using OOTB library tool ugti0402_001

Inch units, this tool length = 3.1 (using analysis -> measure)

I tried MOOG_Show_Globals, and nothing matched up.

(I did find mom_probe_stylus_diameter for the tip dia)

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information