Cancel
Showing results for 
Search instead for 
Did you mean: 

Speacial tool assembly display

Valued Contributor
Valued Contributor

Hey guys,

I tried to introduce special tool at NX 11.  I can see the tool in library. when i tried to see in verify, i changed tool  display with assembly. But i could not see my special tool view. In old versions i was working and also i am using same way. But i doesnt work. Some one can help me? Is there any differences in NX 11?  You can see my way in photos. tool.jpgtool2.jpg

Thanks.

Best regards.

5 REPLIES 5

Re: Speacial tool assembly display

Siemens Phenom Siemens Phenom
Siemens Phenom
Hard to get it from the picture you you shared. are you sure the operation uses the "Kilangic" tool you created? I do not have NX 11 installed, but with newer versions it seems to work.

Yours,
Eddy Finaro
NX CAM Product Manager
Siemens PLM

Re: Speacial tool assembly display

Valued Contributor
Valued Contributor
Yes, i am sure, i used tool which is created.
Highlighted

Re: Speacial tool assembly display

Phenom
Phenom

Does the folder name in the "library\tool\graphics" folder match the libref name?

 

Is assemblies on and enabled under the "file" menu with a check mark next to it?

Glenn Balon
Production: NX 12.0.2 MP10 Primarily CAM

Re: Speacial tool assembly display

Valued Contributor
Valued Contributor

Yes, i can see tool name in library file. Also assembilies is active.

I send you the photo. Please check them. Thank you.1.jpg2.jpg3.jpg4.jpg

Best Regards

Re: Speacial tool assembly display

Valued Contributor
Valued Contributor
Now it works. Thank you so much. i did not have permission to write to graphics file.

Learn online





Solution Information