Cancel
Showing results for 
Search instead for 
Did you mean: 

Spindle and Counter-Spindle setup

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Hello!
I have cse model with spindle and Counter-Spindle, with part and blank for each. When I add nc machine for simulation I can use Use Part Mount. Main part mount in main spindle. How I add part to sub-spindle?
2 REPLIES

Re: Spindle and Counter-Spindle setup

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I'm not sure that's the best way because I'm not a great expert in dual channel, but what I do is once you mount the machine and the workpiece in the main spindle, to add the second piece on the sub spindle, I do it from the machine tool navigator.

 

Sin título.jpg

Re: Spindle and Counter-Spindle setup

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Yes, I can define part for Sub-Spindle setup in Machine Tool Builder Tree. But - a position of part or blank will not changed (and MCS for G54 G55..), and if I want to use sub-spindle - I must to calculate part mount before adding simulation model or move component after it. Not so easy..

 

 

Learn online





Solution Information