Cancel
Showing results for 
Search instead for 
Did you mean: 

Spun outline issue

Master
Master

I have a spun outline that doesn't show the part. If you select part spun outline you can see the profile otherwise all you see is the blank spun outline. It will drive but I just can't see both profiles as I have in every other job I have worked on. Thanks I am in 8.5 with Teamcenter.

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000
2 REPLIES 2

Re: Spun outline issue

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Shaded view or wireframe?

I set the translucency of my spun blank sheets to about 75%, so they can be seen, and the part is visible too.  Works great, except about 50% of the time when an updated happens, one (or both) blank sheets lose their translucency...

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Spun outline issue

Master
Master

This was actually a coworkers file and he had his view set to shaded with no edges. LOL. I never use that so it never entered my mind until today. Thanks Ken!

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Learn online





Solution Information