Cancel
Showing results for 
Search instead for 
Did you mean: 

Step Drill definition

Experimenter
Experimenter

Hi,

 

I have a situation where I have to defined complex cutter and after reading this post I thought it was the way to go. After exporting in the library I tried to go back to them and edit them manually but I couldn't find the "step" definition. Also, when we import some of those tool some have all the previously defined step but some are missing some. I wanted to know where I could find the value where the steps are defined so I could go back and correct the missing information.

 

Thank you for your help and time.

5 REPLIES

Re: Step Drill definition

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

if the tool is in tool_database.dat, then step drills are in segmented_tool_database.dat

 

Note if you use CAM configuration files (...\MACH\resource\configuration\)

there are separate entries for each of the above (plus 2 more for the holder & tracking point files):

 

LIBRARY_TOOL,${UGII_CAM_LIBRARY_TOOL_ASCII_DIR}dbc_tool_ascii.def,${UGII_CAM_LIBRARY_TOOL_ASCII_DIR}dbc_tool_ascii.tcl
LIBRARY_SEGMENTED_TOOL,${UGII_CAM_LIBRARY_TOOL_ASCII_DIR}segmented_tool_ascii.def,${UGII_CAM_LIBRARY_TOOL_ASCII_DIR}segmented_tool_ascii.tcl
Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Step Drill definition

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Without the "close braces" which hose up the display....

 

LIBRARY_TOOL,${UGII_CAM_LIBRARY_TOOL_ASCII_DIR(close brace)dbc_tool_ascii.def,${UGII_CAM_LIBRARY_TOOL_ASCII_DIR(close brace)dbc_tool_ascii.tcl
LIBRARY_SEGMENTED_TOOL,${UGII_CAM_LIBRARY_TOOL_ASCII_DIR(close brace)segmented_tool_ascii.def,${UGII_CAM_LIBRARY_TOOL_ASCII_DIR(close brace)segmented_tool_ascii.tcl
Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Step Drill definition

You should not need to manually edit the library files.  I think it would be safer for you to retireve the step drill you added, edit it, export it, and replace the previous one. 

 

Mark Rief
Retired Siemens

Re: Step Drill definition

Experimenter
Experimenter

I do agree that it would be safer, however it'll be way quicker to edit the tools manually with notepadd++ for about 80 tools rather than do them one by one, but thank you for the advice.

Re: Step Drill definition

Experimenter
Experimenter

I didn't think of checking the segmented_tool_database and it was exactly what I was looking for, thank you very much!

Learn online





Solution Information