Cancel
Showing results for 
Search instead for 
Did you mean: 

Stock box keeps appearing when clicking on operation

Phenom
Phenom

Is this something that can be disabled? AFAIK this is a NX12 feature, NX10 didn't have this. The stock box only appears with cavity mill and adaptive. Clicking on the hole operations behaves as expected.

 

s1.JPGs2.JPG

6 REPLIES

Re: Stock box keeps appearing when clicking on operation

Legend
Legend

I see this same behavior in 11.0.2

You can right button click "replay" to get it to disappear, but yes... very annoying.

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: Stock box keeps appearing when clicking on operation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I'm not sure about NX12 and Adaptive Milling - but in general, you should be able to turn it on and off with one of Customer Defaults, I guess it is this one:

 

2018-02-01_16-38-27.png

 

 

 

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: Stock box keeps appearing when clicking on operation

Legend
Legend

Awesome. I'll give it a try.

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: Stock box keeps appearing when clicking on operation

Phenom
Phenom

Thanks Marek, you've saved me a lot of bad language Smiley Wink

 

Harri

Re: Stock box keeps appearing when clicking on operation

Gears Phenom Gears Phenom
Gears Phenom

nx11 nx 12,

I have it turned on and I have no such display. When I select cavity only cut area and tool path are displayed.

Isnt it something with enabling transfluency?

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Stock box keeps appearing when clicking on operation

Legend
Legend

I had it on... have now turned it off and all is well.

 

No "stock block" showing up when I click the operation in the navigator now.

 

I would have never guessed it from the one line discription, Extended discription was better...

But I had previously looked a few times and never found it...

 

 

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Learn online





Solution Information