Cancel
Showing results for 
Search instead for 
Did you mean: 

Suppressing and Locking a Machining operation in place

Pioneer
Pioneer

Hello all,

Is it possible to suppress a Machining operation and or Locking one.

 

I would like to keep it in place in the program location without moving it to the Unused Items folder.

 

And Lock it to keep it from a regenetaion when geometry changes.

 

Thanks

Phil

3 REPLIES

Re: Suppressing and Locking a Machining operation in place

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello Phil,

 

Select the operation that you what do prevent from regenerate.

Klick right mouse button and select: "Tool Path" > "Lock"

Now the Operation is Locked up and prevented from manipulation.

 

Lock_OP.JPG

 

 

 

 

 

 

If the geometry changes or something forces NX to regenerate the OP, a warning is created

 

Lock_OP_2.JPG

 

After that is is necessary to accept the tool path without regenerate. 

Klick right MB on the locked OP and select "Object" > "Approve"

 

Toolpath is alive again 

 

greetings,

Andre 

 

 

 

 

 

Re: Suppressing and Locking a Machining operation in place

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you checked the context menu of the operation in the operation navigator?

There are options to lock a tool path.

To suppress the tool path, you just need to delete the internal tool path and keep the operation.operation_tool_path_options.PNGLock tool path

 

 

To delete a tool path use the delete menu entry, which is the fourth below the lock entry in the image above.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Suppressing and Locking a Machining operation in place

Pioneer
Pioneer

Thank you. That was quick!

Learn online





Solution Information