Cancel
Showing results for 
Search instead for 
Did you mean: 

Synchronization Manager window size

Master
Master

I was wondering if there was a way for the synch window to be set to a default size and selecting what things to be expanded in it? Like this possibly? Thanks for looking

 

current window.pngcurrent windowdesired window.pngdesired window

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000
5 REPLIES

Re: Synchronization Manager window size

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

unfortunately this is an older dialog, which does not support these "Dialog Memory" feature. So there is no setting to remember the previous size or define a different default one.

 

Thomas

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Synchronization Manager window size

Master
Master

Darn it. Thanks for the information sir.

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: Synchronization Manager window size

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you file an IR/ER, (and post the number here) I'll add a "Me too" IR to it.

 

Note I also have an ER 7116700:

Synch Manager window - maintain selected item as you collapse all/expand all

When working in the synchronization manager, and you can change the different "view modes" (collapse all/expand all/show machine code). If something (in particular a sync event) was selected, it would be nice if it remained selected as you change the display. NX9.0.1 is much better than N7.5, but it still jumps off the selected sync code to an event nearby, instead of leaving the sync event selected.

 

I'm not sure if it is fixed by NX10, but if not, (and this bugs you) you might want to add a "me too" to my ER :-)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Synchronization Manager window size

Master
Master
I tried to add to yours but couldn't find the ER. Maybe I am looking in the correct page. Do you have a link?
Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: Synchronization Manager window size

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What you have to do is file your own IR, and (what I usually put when doing this)

"I'd like to file a 'Me too' ER on ER xxxxx"

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information