Showing results for 
Search instead for 
Did you mean: 

Synchronization Manager


How can i change the output file name and path in synchronization manager? There is no option as in the "normal" post process dialog.


Re: Synchronization Manager

Siemens Phenom Siemens Phenom
Siemens Phenom

as fas I know is there no NX setting to influence this. This can only be handled within the tcl of the postprocessor itself.


Re: Synchronization Manager

Esteemed Contributor
Esteemed Contributor

I write my own custom commands & put in the "end of program" event.

There's a fair amount of logic to consider:

1) Are you posting outside sync manager? (you may or may not want to rename)

2) Is NX posting when the sync manager is starting up? (you do NOT want to rename)

3) Is NX posting from sync manager (to get the final files)? (you DO want to rename)

4) Is post being run as part of IS&V to verify G&M code (vs internal toolpath) (probably don't wnat to rename)


The following variables are a starting point:

global mom_postprocessing_mode
global mom_run_number
global mom_output_file_basename	
global mom_sys_output_file_suffix
global mom_output_file_directory 
global mom_output_file_full_name 

I would suggest using "MOM_output_to_listing_device" to report their values for the various situations above & develop your own logic.


Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled

Learn online

Solution Information