Cancel
Showing results for 
Search instead for 
Did you mean: 

Synchronizing Tool Paths in nx cam

Creator
Creator

How to create Synchronizing  Tool Paths & post process

9 REPLIES 9

Re: Synchronizing Tool Paths in nx cam

Creator
Creator
please kindly anyone reply to me

Use the Synchronization Manager to create multi-channel,...

Community Manager Community Manager
Community Manager

Use the Synchronization Manager to create multi-channel, synchronized motion.  See the help files - there is a section on synchronization at the top level of the CAM help section:

Help>CAM>Synchronization Manager.

Derek Hart
... if we're not having fun, we're not doing it right!

Re: Use the Synchronization Manager to create multi-channel,...

Creator
Creator
I request to you need synchronization video file help, I can easily understand.

Macro program develop post processor

Creator
Creator

Hi

 

         How to Develop 2D Macro program  for post processor and control the tool path in  first motion, please go through the below Macro program output type, 

 

N9000 G61
(*****************************)
(D32.0 R3.0 ENDMILL  C T)
(*****************************)
    #1=-135.8 (FUKASA SHIAGE  D1250-D1197.5/2+120)
    #2=1.50
    #3=91
(T CORE )
    #11=-100.0 
    #12=1.50
    #13=68
(*****************************************************)
   S1000 M03
   G00 Z100.0
   M08
(*****************************************************)
    #4=[#1+[#2*#3]]
N1 G00 X-20.0 Y0.0
   G01 Z#4 F500.0
   G01 G41 D23 Y-16.45 F200.0
   G01 X51.0
   G01 Y16.45
   G01 X-20.0 F300.0
   G40 Y0.0
    #4=[#4-#2]
     IF[#4LT#1]GOTO2
      GOTO1
N2 G00 Z100.0

   G54.1 P2
    #14=[#11+[#12*#13]]
N3 G00 X20.0 Y0.0
   G01 Z#14 F500.0
   G01 G41 D23 Y16.45 F200.0
   G01 X-51.0
   G01 Y-16.45
   G01 X20.0 F300.0
   G40 Y0.0
    #14=[#14-#12]
     IF[#14LT#11]GOTO4
      GOTO3
N4 G00 Z100.0

 

 

 

Thanks

PostBuilder

Re: Macro program develop post processor

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You macro example doesn't seem to have much to do with sync manager ;-)

But anyhow...

 

Writing macro style programs is not something NX does well (or at all) "as installed".

It generally is intended to write the actual NC code to run, with actual values (not variables)

 

Not to say you can't get what you want, because you can.  But it will require adding custom UDEs and a _lot_ of "post magic" to make it happen.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Macro program develop post processor

Creator
Creator

Hi Ken

Thanks to you for yor answering

 

The Macro is not sync Manager,

 

This macro progrm use to 3axis Machine,

 

I need your support to develop Macro progrma for post processor,

How to relate UDE to Macro & control  tool path Depth,

can you explain about the macro?

Re: Macro program develop post processor

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Well, it's not something easily explained in a post on a forum like this.

One could say this is in the "non trivial" category ;-)

 

I would suggest (if you haven't already) taking the Postbuilder/CAM customization training class from Siemens.

 

What you need to develop is UDEs for each operation type to drive the behavior, then LOTS of customization in PB to do the output (actually, it may be easier to ignore PB and just write the .tcl & .def files yourself). 

 

Sorry, but you're asking for something like a month's worth of my time to do this, and that's way more time than I have available.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Macro program develop post processor

Creator
Creator

Hi Ken,

I know the  new develop post processor (UDE ,TCL) for 3 to 5 axis Machine,  No need explain from beginning level of the post, how to customization macro program of post, can you explain how to setup the macro sup file (text file)  to linked post and tool path

Re: Macro program develop post processor

Phenom
Phenom

Your macro seems to be two mill profiles with a loop to mill multiple z depths. Do you want the profile to come from path in CAM? Or are you asking how to make the post output the lines in this macro? Or are you asking how to make the post call this macro that already exists on the control?

 

Macro code is not ideal for any cam system to output. For one thing - replay has to be aware of the motion made in the macro - which is more possible when an integrated simulation reads and understands the logic in macro code (which ISV is capable of.) Still stock updates that cam depends on will not be made.

NX12.02
Windows 10 Pro

Learn online





Solution Information