Cancel
Showing results for 
Search instead for 
Did you mean: 

TCL array with global key

Valued Contributor
Valued Contributor

I am trying to acces a tcl array with a key which is a global variable. Postbuilder won't save such a construction. If I modify this in the tcl file itself the post works just fine. This post also opens without problem, but it won't save. I do see similar constructions though. Procedures LOCK_AXIS and UNLOCK_AXIS are using it.

 

I am using mom_tool_designation but it can be any global variable. A very simple example:

global mom_tool_designation
array set myarray {foo bar}

MOM_output_literal $myarray($mom_tool_designation)

And mom_tool_designation should exist and be "foo" of course to see something. But this is not postbuilders business. I understand that the above construction will get me into trouble if I don't check anything before using it. 

W10 NX12.0.2.9
testing v1847
4 REPLIES

Re: TCL array with global key

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would quote the output:

 

MOM_output_literal "$myarray($mom_tool_designation)"

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: TCL array with global key

Valued Contributor
Valued Contributor

The MOM_output_literal was not the problem. But I tried the quotes anyway, didn't help. What did solve the problem was making some if else statements holding one solution without the key as a global var in it. 

 

Still don't understand why that does work though. 

W10 NX12.0.2.9
testing v1847

Re: TCL array with global key

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That's why almost all my tcl code is in an external (sourced in) tcl file.

 

Almost all my custom commands in the post look like:

PB_CMD_Moog_Do_XYZ { } {
# This does XYZ
# put it is these events:  ...
      Moog_Do_XYZ ;# Call external proc.
}

 

Postbuilder parser stays happy.

Of course, now I have to actually run the post to find all the "dumb programmer tricks", instead of having them found in PB.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: TCL array with global key

Valued Contributor
Valued Contributor

@Ken_A wrote:

That's why almost all my tcl code is in an external (sourced in) tcl file.


 

Agreed, although I would prefer not to put things in an external file. Just to have everything in one place. 

W10 NX12.0.2.9
testing v1847

Learn online





Solution Information