Cancel
Showing results for 
Search instead for 
Did you mean: 

TOOL

Pioneer
Pioneer

FUNDO.jpg

HOW CAN IMPROVE THIS TOOL WAY I WANT TO FINISH THE WALL AND WITHOUT THE TOOL FUND BE JUMPING ON ONE SIDE TO ANOTHER

6 REPLIES

Re: TOOL

Creator
Creator

What i've done before when ive seen this is, set all accuraccy in stock settings to "in tol 0" "out tol .0001"

If that doesnt do it, then also add .0002 stock.

Re: TOOL

Pioneer
Pioneer

FUNDO-2.jpg

DID NOT WORK WILL YOU HAVE ANOTHER OPTION BEST

Re: TOOL

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would change from stepover applied on plane to stepover applied on part, which will improve the tool path and there will be no need to change the tolerance.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: TOOL

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

You might try changing your projection vector to look normal to that bottom surface.

Re: TOOL

Siemens Experimenter Siemens Experimenter
Siemens Experimenter
You can try to modify the Boundary Intol and Outtol, such as 0.001

Re: TOOL

I'm not sure I would want the same cut pattern over the entire cut area.

Have you looked at steep and non-steep settings? The system will use zlevel in the steep areas.

You can see this used in the High Speed Machining tutorial, found in Help > Manufacturing Tutorials.

 

If the part gets complicated, take a look at cut region management. 

Mark Rief
Retired Siemens

Learn online





Solution Information