Cancel
Showing results for 
Search instead for 
Did you mean: 

TRACKING_PLAQUITAS

Saludos cordiales, por favor que me ayuden con el concepto de dirección
del punto imaginario de intersección de la herramienta, estoy muy agradecido.

plaquita.pngRASTREO.png

1 REPLY 1

Re: TRACKING_PLAQUITAS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This really should be moved to the Manufacturing forum

 

But anyhow...

For normal (insert) turning tools, you get to choose what the output coordinates refer to.

This is also shown as the toolpath when you generate or replay the internal toolpath in NX.

i.e....

Do you want the output coordinates (X/Z) to represent the "center of the tip radius" ("0" / "9" in your diagrams) or the "theoretical "point (for typical OD insert in left spindle, upper turret, "2") that you would probably actually touch off the tool to get offsets.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information