Cancel
Showing results for 
Search instead for 
Did you mean: 

Ta6V pocketing toolpath

Experimenter
Experimenter

Hi everybody,

 

I would like to modify the toolpath of a titanium pocketing.

The strategy is as follow :

 

drilling a hole Ø59

roughing with helical mill Ø50

finition with mill Ø20

 

The toolpath of the roughing doesn't suits me (picture below), because engagement is not constant (the helical mill will break in the angle). I would like a "snail" toolpath in order to have constant engagement of the mill.

Anyone know which operation/option I should use to obtain this result?

 

Thank you in advance

(the program is in POCKETING_FAO.prt)

 

Laurent

 

Rough.PNGRoughing toolpath

 

4 REPLIES

Re: Ta6V pocketing toolpath

Genius
Genius

Hello @LaurentW

 

You don't mention what version of NX you are using?

 

I have access to NX11 and using Adaptive roughing think the below image is what you are looking for but this is not fully available until NX12 as I understand it?

 

Adaptive_roughing.JPG

 

You can using Trochodail and playing with the setting and using smoothing get a good toolpath but not what you are really looking for.

 

 

Unable to play video. Please try again later.
(view in My Videos)
 

I also tried a cheat using Hole Milling and then rest milling which I think is ok (ish) have a look at the below.

Hole_milling.JPGRest_milling.JPG

 

Unable to play video. Please try again later.
(view in My Videos)

 

Not sure if any of the above is what you were looking for but hopefully it may have been of use.

 

Have a good day.

Regards

Dave
NX10.0.3MP13
NX11.0.1
Production
TC10
Vericut 7.3,7.4.1,8.0.2

Re: Ta6V pocketing toolpath

Experimenter
Experimenter

Thanks Dave,

 

I'm working on NX10.0.3.

 

In fact the first solution is interesting.

 

I tried another solution, by cheating and use a larger pocket, reduce it by defining the real pocket as "check geometry". I used the operation "Fixed axis surface contouring", drive method "spiral".

I obtain something looks like what I want but it's still not perfect. I would like to have an option spiral + "add a finish pass" but looks like it doesn't exist.

May be I will try to concat 2 operations without retract/engage movement to finish the coutouring but I'm not very happy with that.

 

spiral.PNG

 

Re: Ta6V pocketing toolpath

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

This should be what you want!

 

2017-07-31_11-13-36.png

Re: Ta6V pocketing toolpath

Experimenter
Experimenter

Yes it seems good, how did you do that?

 

Learn online





Solution Information