Cancel
Showing results for 
Search instead for 
Did you mean: 

Tapping

Experimenter
Experimenter

Hi

This is esprit tapping programme. I want to recreate this operation in Nx. I haven't done tapping before in NX. Which is the best operation to do it in NX. Could you help me with this.

 

Regards,

Ram

2 REPLIES 2

Re: Tapping

Phenom
Phenom

Sorry I don't understand "This is a esprit tapping programme..." if you want to have a cycle , hole making operations should be good...

help Nx 11 : Hole machining operations

Production: NX11.0.2.7,VERICUT 8.1.2
Development: Tcl/Tk, Gnuplot
www.adgroupe.com

Re: Tapping

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Sedco,

 

thank you for your question.

 

You can find the Tapping template under the Type hole_making.

2017-08-23 10_12_32-NX 12 CAM_nx1201 Build CAM_nx1201.127 - Manufacturing.png

 

 You can edit the parameters for the tap cycle here:

2017-08-23 10_15_57-NX 12 CAM_nx1201 Build CAM_nx1201.127 - Manufacturing.png

 

The depth, pitch and other important values are typically automatically recognized through NX CAM out of the part model. They can be manually adjusted in the feature geometry dialogue.

 

2017-08-23 10_20_41-NX 12 CAM_nx1201 Build CAM_nx1201.127 - Manufacturing.png2017-08-23 10_21_17-NX 12 CAM_nx1201 Build CAM_nx1201.127 - Manufacturing.png

 

If you have any further questions, please let me know. Maybe a good idea would be to get an initial training. Ask your reseller about it. There is also much more that you can do in NX CAM. For example Feature Based Machining, where Holes and geometries are automatically recognized and the necessary operations created.

 

Cheers,

Alexander

 

Lead Product Manager - Mold & Die

Learn online





Solution Information