Cancel
Showing results for 
Search instead for 
Did you mean: 

Template Doesn't remember tool Nx10

Creator
Creator

Hi 

 

When i insert an operation from a template that i created, it doesn't remember the cutting tool ?

 

I've never had a problem in previous version but its been a while since I've done any template work & i can't remember how to remember the tool

 

Does anyone have any suggestions ?

 

Thanks

 

 

 

 

 

 

 

3 REPLIES 3

Re: Template Doesn't remember tool Nx10

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi

 

Have you already set up the template settings in the template-file ? 

 

Template.pngtemplate2.png

Re: Template Doesn't remember tool Nx10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is also a customer default to load the tools if an operation template is used, but it is marked as legacy, so it might not have any effect.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Template Doesn't remember tool Nx10

Creator
Creator

Hi 

 

Yeah i have already set up the template

 

2018-06-30 12_47_21-NX 10 - Manufacturing - [FeelerVMP50_V1.0.prt].png

 

but i still get no tool

 

2018-06-30 12_50_23-B Ear Planar Mill - [B_EAR_PLANAR_MILL].png

 

but if i insert previous created geometry with operations, using the same tool it works fine

 

2018-06-30 12_52_23-NX 10 - Manufacturing - [Feeler_Manifold_Template_mfg1.prt (Modified) ].png

 

It doesn't seem to matter what tool I change the operation to use, it always comes in without a tool  

 

Thanks

 

 

Learn online





Solution Information