Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Template Image

Valued Contributor
Valued Contributor

Another Topic: What color should I choose in my bitmaps to get a transparency if I choose the Operation in template? Earlier it was RGB 192,192,192. Now this does not work anymore.

 

 2015-06-22 12_24_09-Create Operation.png

 

 

Werner
Production: NX12.0.2, FBM | TcUA 11.4.0.6
Development: VB.NET, Tcl/Tk

Re: Template Image

Genius
Genius

Hi jobe,

 

NX help:

Home->System administration->Customizing the NX installation->Customizing the NX interface:

 

Transparency

For a background transparency color on 24-bit bitmaps use magenta (255, 0, 255). NX treads magenta as transparent for all high-quality bitmap files stored as 24-bit (16 million color) and 8-bit (256 color), ans light grey as transparent for all bitmap files stored as 4-bit (16 color).

 

There is also some methioning regarding partial transparency.

 

The non 24-bit bitmaps can just be handled on Windows systems.

Best wishes,
Joachim

In production NX 12.0.1.7 D2
In testing NX 12.0.1.7 MP4

Re: Template Image

Valued Contributor
Valued Contributor

Hello!

 

I think NX10 does not know the documentation Smiley Sad In NX8.5 the transparency worked.

 

2015-06-22 15_28_53-Geometrie erzeugen.png

 

In NX10:

2015-06-22 15_29_21-Create Geometry.png

 

one of the backgrounds should be white and the other one like this:

 

2015-06-22 15_29_21-Create Geometry.png

Werner
Production: NX12.0.2, FBM | TcUA 11.4.0.6
Development: VB.NET, Tcl/Tk

Re: Template Image

@jobe -

When you get the bitmap missing message, is there any more detail in the syslog - like the file path it is lookin in?

In your syslog, what is UGII_BITMAP_PATH pointing to?

 

And just confirming - this discussion is only about the Create dialog in CAM. For ribbons and the rest of the UI, it is standard NX customization rules for finding and displaying icons. 

Mark Rief
Retired Siemens

Learn online





Solution Information