Cancel
Showing results for 
Search instead for 
Did you mean: 

The PLM XML Document failed to load when importing Solidworks .sldprt

Legend
Legend

Is this because the files are created in a newer version?

I'm using NX10.0.1


Dennis Rathi
Creations Unlimited
6 REPLIES

Re: The PLM XML Document failed to load when importing Solidworks .sldprt

What version of Solidworks are they files saved in?

Is this with File --> Open? Or import?

After the message, what happens? Is the file still brought in to NX?

Mark Rief
Retired Siemens

Re: The PLM XML Document failed to load when importing Solidworks .sldprt

I have the same problem, using File -> Open.  Not sure of the SolidWorks version (customer supplied data), but I am also running NX 10.0.3.5.  The file is not brought into NX.

Re: The PLM XML Document failed to load when importing Solidworks .sldprt

These are the supported SW versions.

 

NX Release Supported solid works version
NX 8.5 SW 2012
NX 9 SW 2012
NX9.0.3 MP SW 2015
NX 10 SW 2014
NX 10.0.1 SW 2015

 

If you are getting an error, and the SW file is not newer than shown above, please log a call with GTAC so that it can be investigated.

Mark Rief
Retired Siemens

Re: The PLM XML Document failed to load when importing Solidworks .sldprt

I have an open PR for the issue, 7598976 generated from IR 7598976.  I'm not sure of the version of SW file I was using, but I got the error in NX 10.0.3.

Re: The PLM XML Document failed to load when importing Solidworks .sldprt

Genius
Genius

Any Solutions for this?

 

I have NX 10.0.2 and NX 10.0.3 and was able to read SolidWorks files last week  Today, they won't load anymore with "The PLM XML document failed to load" error.

 

My computer was updated with the Visual C++ Redistibutable for Visual Studio 2015 to be able to run 2015 applications.  Could that be related?

 

It also leaves it also leaves empty .x_t files and log files behind.

 

<DtkApiVersion>152<\DtkApiVersion>
Process Conversion without healing
<FileName>D:\Belt.sldprt <\FileName>
<FileVersion>Official version for SolidWorks 2009 <\FileVersion>
<UnitScale>1<\UnitScale>

Conception Unit Scale from Model to MM : 1

Converting Component Name =D:\Belt.sldprt

Error dtkErrorEmptyFile in ReadComponent : Belt - 8th Axis
TITLE ==
SUBJECT ==
AUTHOR ==
KEYWORDS ==
COMMENTS ==
NAME == Administrator
LAST_RECORD == Fri Jan 31 16:26:21 2014
CREATED == Fri Jan 31 16:26:21 2014
TITLE ==
SUBJECT ==
AUTHOR ==
KEYWORDS ==
COMMENTS ==
NAME == Administrator
LAST_RECORD == Fri Jan 31 16:26:21 2014
CREATED == Fri Jan 31 16:26:21 2014
Warning : Unable to produce file due to error 22

Reading file
__________________________________________
ENTITY LIST
__________________________________________
Count Entity Type
__________________________________________
1 DTK_PROTOTYPE
1 DTK_CATALOG
__________________________________________
2 TOTAL
__________________________________________
<OutPutFileName>D:\Belt.sdlprt.x_t<\OutPutFileName>
<OutPutFileSize>0<\OutPutFileSize>

Start API : 09:35:36
End API : 09:35:37
API started during : 1sec

 

Re: The PLM XML Document failed to load when importing Solidworks .sldprt

My IR was closed.  They said there were files missing in the orignal .SLDASM file.  I was not able to try again, as the file was sent from a customer.

Learn online





Solution Information