Cancel
Showing results for 
Search instead for 
Did you mean: 

The controls that are working with conversational code, can interpret g-code of NX CAM?

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I have the issue of some lathes with the following controls,

Mori Seiki SL35 Fanuc Series 15T
Daewo Puma 400 Fanuc 18iT
DMG Mori SL-603/1000 control Mori Seiki F32iB

I have doubt because the owner does not know if his machines can read of 2 types of codes, G and conversational. The best way would be to test a program G.
Before that I want the opinion of the community, are there controls that can work both ways or how does this work?

2 REPLIES 2

Re: The controls that are working with conversational code, can interpret g-code of NX CAM?

Legend
Legend

Have worked on many Mazatrol Mills 3,4 and 5x, Turn Mills and Mill Turns.

Went seamlessly from both styles of programming We ran about 50/50, Conversational vs G-Code.

 

There were some parameters we had to set that changed the way the Tool Data was used or picked up (Tool Length and Tool Diameter)... We made the G-code use it the same way the conversational did.

 

Could use the same tools in either format.

 

I would imagine other controls can also go back and forth no issue.

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: The controls that are working with conversational code, can interpret g-code of NX CAM?

Solution Partner Creator Solution Partner Creator
Solution Partner Creator
Thanks

Learn online





Solution Information