Cancel
Showing results for 
Search instead for 
Did you mean: 

The differences between the mom_toolpath_time and the real machine time

Creator
Creator

Hi,

 

I put to postprocessor the variable mom_toolpath_time, and for example it give me 82 minutes. But when the program goes on the machine, it takes a lot longer - about 200 minutes..I found two reasons of this. First when we use operation who had many rapid moves - here I have a question what is the default rapid speed in Feeds and speeds rapid output? How can I change this for exapmle 2500mm/pm (can't change to G1 becouse postprocessor gives me colision movements)

 

Secondary reason, in a advance shapes when i use contour area (now there is a few G0 movements but the g-code is much more larger with many lines of codes). I know that machine need a slow down and acceleration on shapes to cut material but is that some way to calculate this?

 

 

 

3 REPLIES

Re: The differences between the mom_toolpath_time and the real machine time

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Here you can set how fast rapid motions are:
(You might be also interested in Tool Change time)2017-10-12_13-41-02.png

  

 

 

Referring to second question, you can take into account also acceleration and deceleration of the machine. You can do it in ISV. Obviously first you need to provide all this data specific to your machine like: max velocity, max acceleration and deceleration etc (for each axis!). Results might be very precise!

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: The differences between the mom_toolpath_time and the real machine time

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The times reported in NX (vs. in IS&V) have always been "off"

Not just for accel/decel, but other things as well.

 

NX10.0.3.5 MP16

Converted an operation from deep hole drill (G83) to regular drill (G81) (Times from the "time" column in the ONT)

G81 operation time: 30 sec.

G83 operation time: 30 sec.

To quote the old "Laugh in" TV show: "Verrryyy Interesting!"

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: The differences between the mom_toolpath_time and the real machine time

Creator
Creator

Thx Marek. It's works Smiley Very Happy

Learn online





Solution Information