Cancel
Showing results for 
Search instead for 
Did you mean: 

The "check geometry" is not recognized 2

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello

 

 

Last time after question


it is addition question

Image1.JPGImage3.JPGImage22.JPG

 

 


sayd "Paul_Hartrick"


'I still notice that the tool holder is interfering with the check surfaces though.'

 

 

My customer is to tell same question.


Why does not the holder recognize it as a check geometry?

 

6 REPLIES 6

Re: The "check geometry" is not recognized 2

What operation type?

What are the collision checking and clearance settings?

Mark Rief
Retired Siemens

Re: The "check geometry" is not recognized 2

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Image6.JPG

Operation Type : Variable Contour / Drive Method : Boundary

Image4.JPG

 

Collision checking

Image3.JPG

 

Clearance Setting

Image5.JPG

Highlighted

Re: The "check geometry" is not recognized 2

Genius
Genius

Hello @micro_73

 

The only way that I could get the tool to avoid the Check Geometry was to up the clearance tolerance on the Check Geometry itself? any change to the holder clearance was ignored?

 

One thing that will need reporting to GTAC is that when you edit the Check geometrys clearane to .5 or 1mm then hit ok and try and generate the operation it throughs a Internal Error Alarm and you have to hit ok to close the operation and reopen it and then you can generate it?

 

Regards

Dave
NX10.0.3MP13
NX11.0.1
Production
TC10
Vericut 7.3,7.4.1,8.0.2

Re: The "check geometry" is not recognized 2

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello CAM_Jockey

 

Thank you for the reply. ^^

I will test it in the way you have guided it.

 

additional one question

By default, Does not "Fixed contour" operation recognize holder check  ?

 

Regards

Re: The "check geometry" is not recognized 2


@micro_73 wrote:

 

additional one question

By default, Does not "Fixed contour" operation recognize holder check  ?

 



What do you want to check?

Holder is checked against part and check if the option is turned on:

 check tool and holder.jpg

Mark Rief
Retired Siemens

Re: The "check geometry" is not recognized 2

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

 Sorry i was late.

 

I have found that the above option(Check Tool & Holder) are different for different drive types.

Only "Area Milling" have above option.(Check Tool & Holder)

Other Drive Methods don't have this option.

To have other "Drive Methods" is 'Check Tool above Ball'. 

So the question i have is...

Whether to check "Holder" When I use the option(Check Tool above Ball).

 

Regards

Learn online





Solution Information