Cancel
Showing results for 
Search instead for 
Did you mean: 

The "check geometry" is not recognized

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

capture2.JPGcapture1.JPG

 

Why do not check geometry recognize ?

 

NX Ver : 11

4 REPLIES

Re: The "check geometry" is not recognized

Siemens Genius Siemens Genius
Siemens Genius

Hi micro_73

In cutting parameters --> Containment turn on "Check Tool above Ball". I still notice that the tool holder is interfering with the check surfaces though. A bit more investigation is needed. Maybe by the GTAC team.

Regards

Paul

Re: The "check geometry" is not recognized

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter
Thank you.
your speedy reply

Re: The "check geometry" is not recognized

Esteemed Contributor
Esteemed Contributor

In the check geometry, have you checked the topology dialog for the face vectors?

Make sure to unify then face vectors and point them into the right direction.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community

Re: The "check geometry" is not recognized

Siemens Genius Siemens Genius
Siemens Genius

Hi Stefan,

I did do that. I also thicken the surface to make a solid and added the solid as check. Still same issue. Not sure what is happeneing.

Paul

Learn online





Solution Information