Cancel
Showing results for 
Search instead for 
Did you mean: 

To all experts in FLOOR_WALL

Valued Contributor
Valued Contributor

I work with floor_fall and I'm using the 3D-IPW as workpiece. If I have the following situation

2019-08-09 13_03_29-NX 12 - Fertigung.png

the last of my toolpathes differs to the other ones. Is there a possabillity if working with 3D-IPW to tell the system to generate the tool-pathes still the same as the first one? Thanks to all.

Werner
Production: NX12.0.2, FBM | TcUA 11.4.0.6
Development: VB.NET, Tcl/Tk
3 REPLIES 3

Re: To all experts in FLOOR_WALL

Legend
Legend

Is there a radius on your part it is staying away from?

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: To all experts in FLOOR_WALL

Valued Contributor
Valued Contributor

No radius. What you see on the picture is the IPW from operations before.

Werner
Production: NX12.0.2, FBM | TcUA 11.4.0.6
Development: VB.NET, Tcl/Tk

Re: To all experts in FLOOR_WALL

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you using the Profile cut pattern to cut the outside walls?

 

More information about your Floor & Wall op settings is needed to advise you about this.

Learn online





Solution Information