11-05-2015 01:54 PM
First I apologize as I'm not an NX programmer. Our programmer is new to NX, so I'm trying to help out...
Is there options in NX CAM to create tool paths for text using a single line font or equivilant as opposed to actually machining the model's True Type font shaped extrude feature? We'd like to just use a single line font as the center line for a tool path to engrave text into electrodes, while letting the cutter shape and depth create the cross section of the text.
If possible, could someone provide me with NX's terminology so I can better search for information to pass on?
Kind Regards,
Matt
Solved! Go to Solution.
11-05-2015 02:32 PM - edited 11-05-2015 02:38 PM
On basic engraving I just create a note:
Slimfont
Then the PLANAR_TEXT operation
Tool Path:
11-06-2015 10:24 AM
11-06-2015 02:56 PM
A couple more tips...
If the surface is not planar, use contour_text operation.
If the designers create drafting notes, and they disappear because of view dependency, have them use PMI notes instead.