Cancel
Showing results for 
Search instead for 
Did you mean: 

Tool Path Visulization - Replay not diaplaying path.

Hello All,

In Tool Path Visulization - Replaying an operation does not diaplay the path.  I have to change the tool trace mode to get it to display which leads me to believe it's bugged.

 

Is anyone else experiencing the same behavior?

 

NX 12.0.2
4 REPLIES
Highlighted

Re: Tool Path Visulization - Replay not diaplaying path.

If the Tool Trace is set to Tool Tip, is the path displayed?

Mark Rief
Retired Siemens

Re: Tool Path Visulization - Replay not diaplaying path.

Yes, tool tip is the default.  I have to change it to ball center or none then I go back to tool tip.

NX 12.0.2

Re: Tool Path Visulization - Replay not diaplaying path.

Sometimes it works but frequently I have to use the pull down to get it to display properly.  I usually concern myself with bigger issues but when I have the time I investigate my looong list of nagging bugs.

Smiley Wink

NX 12.0.2

Re: Tool Path Visulization - Replay not diaplaying path.

I have not seen this. If you can catch it in the act, please log something wiht GTAC.

 

Mark Rief
Retired Siemens

Learn online





Solution Information