Cancel
Showing results for 
Search instead for 
Did you mean: 

Tool Path of Follow Periphery pattern

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

 

I used the Periphery pattern as a pattern.

However, a tool path is created as shown below.

 

33.jpg

 

 

I do not want to create that extruded tool path.


Is there a way to prevent the stepover value from being generated without changing it?

2 REPLIES

Re: Tool Path of Follow Periphery pattern

Siemens Legend Siemens Legend
Siemens Legend

Verify the Stepover value. You might want to decrease that a bit.

NX generates these moves when the stepover is that large that it would generate little islands in the corners.

As far as i know it cannot be suppressed, and as far as i could imagine, you don't want the islands also.

 

Regards,

Gerrit Koelewijn

Re: Tool Path of Follow Periphery pattern

Gears Legend Gears Legend
Gears Legend

2 options for this:

 

1: Decrease the stepover (like Gerrit said)

2: Use Cutting > Corners > Smoothing > All Passes

 

Best would be to use both options.

If you only use the corners option than at least the tool will not dive into the corner, but makes a circulair sweep through.

overlap.png

Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Learn online





Solution Information