Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Tool compensation in curve drive

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hey,

I have an operation, when I use Curve as drive. The path is specific, its helisa in the cone schape.

1.PNG

 

I try to output compensation, but I cant :/ I try every operation, but only the curve drive ensure me the right path.

I try also offset the wall and project 3D curve and do the operation on it, but like on the picture below, it doesn't work. 


2.PNG

 

Is any other idea to do this?

 

Best regards,

Jack29

5 REPLIES 5

Re: Tool compensation in curve drive

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Starting with NX 10 use HOLE_MILLING from the hole_making operation template.

Starting with NX 11.0.2 you should also be able to use FLOOR_WALL for helical milling.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Tool compensation in curve drive

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Okay, the problem was solved. I add to NC code RR for tool compensation and machine do it correctly. 

Re: Tool compensation in curve drive

Siemens Legend Siemens Legend
Siemens Legend

FYI - to avoid this kind of resulting path use projection direction- away from line and select the centerline. Apperently you had the projection along tool axis and it is hard for the system to project stadily down a vertical wall.

 

My 2 cents, 

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Re: Tool compensation in curve drive

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

WOW, it is working, thanks a lot! I must more explore the Projection vector bar Smiley Very Happy 

It would be even better, if the toolpath was output with contact data, because it didn't work at the moment.

Re: Tool compensation in curve drive

Siemens Legend Siemens Legend
Siemens Legend

Have you turned on the contact output in the Non Cutting dialog >> More tab? I tried and in seems that the contact data is produced properly. second you have to check that your post processor support it.

 

Yours,

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Learn online





Solution Information