Cancel
Showing results for 
Search instead for 
Did you mean: 

Tool library NX12

Valued Contributor
Valued Contributor

Hello

 

I have installed NX 12 without any customisation. I try to export a tool in the library. Now i get some error messages:

 

The first message is by exporting the tool:

2018-02-09_11h36_51.png

 

 

 

 

 

But it creates the tool in the tooldateabase.dat

 

If i load from the library there will be this error displayed:

 

2018-02-09_11h37_07.png

 

 

 

 

This is in NX12.0.0.27 MP2

I added the syslog

 

Thank you for your help Smiley Happy


Production: {NX 10.0.3.5 MP18}
Testing: {NX 12.0.2.9 MP03}
3 REPLIES

Re: Tool library NX12

Siemens Legend Siemens Legend
Siemens Legend

I just tested in my OOTB NX12 install (12.0.0.27) in both INCH and MM setups and was able to create a tool, import, and withdraw. The only thing I can think of, are you are trying to use an older version of tool_database.dat instead of importing it into the current NX 12 version.

Re: Tool library NX12

Valued Contributor
Valued Contributor

Thank you for your answer.

I installed NX 12 new and everything is fine Smiley Embarassed

 

Wish you a nice week.

 


Production: {NX 10.0.3.5 MP18}
Testing: {NX 12.0.2.9 MP03}

Re: Tool library NX12

Experimenter
Experimenter

hello

could you pleas tell if this error apply when you coustomize the tool data file for NX10 and try too reaload 

thanks

Learn online





Solution Information