Cancel
Showing results for 
Search instead for 
Did you mean: 

Tool path end points color

Valued Contributor
Valued Contributor

Hey friends, 

 

Since NX10.0.2 tool path end point changes according to toolpath color.

Is there any customer default or preference which set the symbol to a specific color ?

It was more clear to see this symbol according to the specfic color.

 

Before NX 10.0.2

image002.jpg

 

 

NX 10.0.2

image001.jpg

1 REPLY 1

Re: Tool path end points color

This was changed in 10.0.2 to display the points inthe same color as the path.

This makes it easier to differentiate when multiple paths are displayed together.

Mark Rief
Retired Siemens

Learn online





Solution Information