Cancel
Showing results for 
Search instead for 
Did you mean: 

Tool tracking point

Pioneer
Pioneer

Do you guys know about tool tacking point (TOOL ANGLE AND RADIUS OF P9)? Thanks!

Capture969696.JPG

-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!
3 REPLIES

Re: Tool tracking point

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

From my experience, that was used when using CLS files and old (GPM/MDF) posts.

Note there is a long standing "on again"-"off again" issue with whether or not TLANGL and RADIUS were output on the tool definition line in the CLS. (it has vascillated many times over the years)

My Postbuilder posts don't require it set, so I pretty much ignore it now

 

Why were you interested in using it?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Tool tracking point

Pioneer
Pioneer

When we use P9 tracking point in operation?

-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!

Re: Tool tracking point

Gears Phenom Gears Phenom
Gears Phenom

The use of the tracking points depends on how your establishing the tool offsets at the machine and how your operators expect the see the positions in the NC program.

 

Are you compensating for the tool nose radius at the machine control? if so then use P9 and the output in the program will be the center of the tool nose radius.

 

Are you touching off the tools with a probe? Then you will need to select the tracking point that corresponds to the touch off point.  This will also change the way the motion in the program is output. It will reflect the tracking point.

John Joyce, Manufacturing Engineer,
Senior Aerospace Connecticut
www.senioraeroct.com
Production: NX11.0.2.7, Vericut 8.0.3
Development: Tcl/Tk
Testing NX12.0

Learn online





Solution Information