Cancel
Showing results for 
Search instead for 
Did you mean: 

Toolpath Special in NX

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Dear,

I have a vertical wall or not vertical , it not close, i want create a toolpath the same picture. I can created it on MasterCAM but how i can creat it on NX ? Please help me

Untitled.png

4 REPLIES 4

Re: Toolpath Special in NX

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Possible. But you must to use ugopen, user defined drive method.

Re: Toolpath Special in NX

Legend
Legend

Generic Motion

 


Dennis Rathi
Creations Unlimited

Re: Toolpath Special in NX

Legend
Legend

Hi @Nguyennhotu,

Attached I'm sending a video showing how you can create this kind of toolpath for a 2D profiles.

I hope it helps.

Jean Marcel
PLMPRO
www.plmpro.com.br

Re: Toolpath Special in NX

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

I have done this using the ramp angle engage to make this type of cut in planer mill.  If this is a contour operation then you could create the 2-D toolpath in planer mill and then use the TOOL-PATH Drive method to define the projected drive path, not my 1st choice.  I cannot download external files so I could not see the other method described.

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Learn online





Solution Information