Cancel
Showing results for 
Search instead for 
Did you mean: 

Toolpath contains unsupported location - cam Robotic

Valued Contributor
Valued Contributor
Hi together, we are starting in NX Cam Robotic and we are facing the above mentioned failure, when we want to apply the robot rules. The toolpath contains two circles which could be the problem, but we don`t why. As operation we use planar mill. When we create only a line and apply the robot rules everything works fine. Can someone give me a hint! Thanks Frank
1 REPLY 1

Re: Toolpath contains unsupported location - cam Robotic

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I can't get an NX license right now, but...

You can (I think - I can't get a license right now, and I can't seem to find it in  the docs) determine if it is an arc output issue, or another issue, by (in the planar mill op) turning the output mode to "linear only" (vs "arc - perpenicular to tool" or whatever it reads).

This will result in all linear motion.

 

Maybe docs are:

https://docs.plm.automation.siemens.com/tdoc/nx/12/nx_help#uid:machine_control_motion_output

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information