Cancel
Showing results for 
Search instead for 
Did you mean: 

Toolpath motion change from arc to line

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello all,

I have created a toolpath for the part as below, The edge of part is Arc (R)

          When R=2000 -->Motion output type arc

                    R=4000-->Motion output type line

Where I set in NXCAM  to R=4000 then motion output type = arc

Please see video in attched file for detail.

Thanks

 

Untitled.png

2 REPLIES 2
Highlighted

Re: Toolpath motion change from arc to line

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

hi all,

I've found a way to set

1.png

Re: Toolpath motion change from arc to line

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Just in case you see it later... Note that the post (Circular move event) also has a max (and min) arc radius.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information