07-04-2015 08:10 AM
Hello all,
I have created a toolpath for the part as below, The edge of part is Arc (R)
When R=2000 -->Motion output type arc
R=4000-->Motion output type line
Where I set in NXCAM to R=4000 then motion output type = arc
Please see video in attched file for detail.
Thanks
Solved! Go to Solution.
07-04-2015 12:04 PM
hi all,
I've found a way to set
07-06-2015 09:46 AM
Just in case you see it later... Note that the post (Circular move event) also has a max (and min) arc radius.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled