Cancel
Showing results for 
Search instead for 
Did you mean: 

Tools saved as component, why?

Valued Contributor
Valued Contributor

I am upgrading from NX12.0.0 to NX12.02. Most of the configuration works. But, for some reason the tools used in operations are save as a component in my machine setup assembly. Simple tools, not solid tools.

 

You won't notice, the tool is not visible in the assembly navigator. But after closing all parts and opening it again the tool is missing, while it wasn't even visible in the assembly before! And to be honest, I don't want is as a component to start with.

 

W10 NX12.0.2.9
testing v1847
7 REPLIES

Re: Tools saved as component, why?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

for me this sounds like a problem, I would like to ask going in contact with GTAC about that topic.

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Tools saved as component, why?

Siemens Phenom Siemens Phenom
Siemens Phenom

Is this issue specific to certain operation types? Or does this happen with every tool used with every operation? Or is it simply every tool regardless of whether it is associated with an operation?

Re: Tools saved as component, why?

Valued Contributor
Valued Contributor
Yes, I already did. I could reproduce it with an OOTB machine setup.
W10 NX12.0.2.9
testing v1847

Re: Tools saved as component, why?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Ahh.. yet another bug that comes up, is fixed, then comes up again, then is fixed again, repeat ad nauseum (sigh...)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Tools saved as component, why?

Legend
Legend

Did see it happen in 12.0.1 last week... just a random tool

Was in verify. Closed verify... tool stuck around.

 

Don't remember seeing it in 11.

Happened a bunch in 10

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: Tools saved as component, why?

Legend
Legend

I turned this in under the EAP program. I think they found the problem but not sure when fix is released.

 


Dennis Rathi
Creations Unlimited

Re: Tools saved as component, why?

Siemens Creator Siemens Creator
Siemens Creator

Hi Thamos,

 

Probably it is same as PR#9191199.

 

Thanks,

Runlei

Learn online





Solution Information