Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Tracking Data with CHAMFER_MILL-Tool and ZLEVEL_PROFILE missing

Valued Contributor
Valued Contributor

Hello, is it the intention on SPLM to have no possabillity to give Tracking Datas if I work with an CHAMFER_MILL-Tool an ZLEVEL_PROFILE:

 

2016-03-29 15_36_11-Non Cutting Moves.png

 

Compared to PLANAR_PROFILE:

 

2016-03-29 15_38_07-Non Cutting Moves.png

 

The problem is, if I want to use ZLEVEL_PROFILE without I can give the Tracking Data SYS_OD_TIP, NXCAM calculates with the Diameter of SYS_OD_SHOULDER:

 

2016-03-29 15_34_49-NX 10 - Manufacturing - [D1791494_0 (Modified) ].png

 

Werner

Werner
Production: NX12.0.2, FBM | TcUA 11.4.0.6
Development: VB.NET, Tcl/Tk
1 REPLY 1

Re: Tracking Data with CHAMFER_MILL-Tool and ZLEVEL_PROFILE missing

FYI I won't have an answer until next week, when the Product Manager returns from vacation Man Happy

Mark Rief
Retired Siemens

Learn online





Solution Information