Cancel
Showing results for 
Search instead for 
Did you mean: 

Tracking Point in NX and tool offset on a Lathe Machine

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi.

I am machining a component with the below tool in a vertical 2-axis Lathe.

2.png

 

For the convenience, I have used the P9(Refer image) as my tracking point.

Now,

Do I need to place offset equal to the radius in the Machine to compensate the distance between tracking point and the actual cutting edge?

 

Please guide and reccomend!

 

Also refer the attachment.

1 REPLY 1

Re: Tracking Point in NX and tool offset on a Lathe Machine

Valued Contributor
Valued Contributor

The output should be based off of that tracking point. If you have 0 for offset as you mention, the person at the machine will have to offset their tools. If you put in an offset equal to the radius, then the person at the machine just need to touch off the tools. Then again it would be the same result as just setting your tracking point to p2 or 3.

Using NX 8.0.3.4

Learn online





Solution Information